AXIS#.IL.FOLDWTHRESH

Description

AXIS#.IL.FOLDWTHRESH is the warning level of the current foldback algorithm. When AXIS#.IL.IFOLD drops below AXIS#.IL.FOLDWTHRESH and foldback is active, a warning is generated.

To ensure that the current foldback warning level is never reached, AXIS#.IL.FOLDWTHRESH should be set well below the continuous current value for both the drive and motor, namely AXIS#.ICONT and AXIS#.MOTOR.ICONT respectively. You can also set the AXIS#.IL.FOLDWTHRESH value to zero.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0 to 500 Arms

Default Value

Drive_IPEAK

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.FOLDWTHRESH

500ah

0ah

Signed32

-

1000:1

Read/Write

No

AXIS2.IL.FOLDWTHRESH

510ah

0ah

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5807

1

5807 (0x16af)

AXIS1.IL.FOLDWTHRESH

Signed32

Read/Write

Yes

71343

2

5807 (0x16af)

AXIS2.IL.FOLDWTHRESH

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.FOLDWTHRESH

5807

Float

Read/Write

-